This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART Bootloader code

Hi there,

I want to add UART boot loader for my application. I have gone through the TIVA bootlaoder guide and have also gone through boot serial example as well.  My only query is that how I need to add UART Bootloader in my application. I am not much familiar with TI bootloader. If possible kindly could you please provide me some code containing UART bootloader such that firmware can be updated via UART.

I have also gone through boot demo uart example but I don't understand it much. I also don't know I need to create a linker file for this. Actually I want to add UART boot loader in my application such that when a certain command let say "update" is sent from PC, It should start the update process. Kindly could some body provide me some code such that It contains some application code as well as the required boot loader code. Actually I don't know how I need to add boot loader code at top of my application.

I shall be very thankful for your support.

Regards,

Mohsin