This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ARMv7 CPSW driver, poor TX performance

We are running the CPSW driver on a TI platform using linux 2.6.37.  We are seeing about 300Kbps transmit through the eth0 device.  Can anyone explain why the throughput is slow?

Thanks ahead of time,

K-

Processor       : ARMv7 Processor rev 2 (v7l)
BogoMIPS        : 599.65
Features        : swp half thumb fastmult vfp edsp neon vfpv3
CPU implementer : 0x41
CPU architecture: 7
CPU variant     : 0x3
CPU part        : 0xc08
CPU revision    : 2

Hardware        : touchlink
Revision        : 20006
Serial          : 0000000000000000