This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Blinky Program does not run automatically after power on



I import the blinky example program form TI suite and it runs correctly.

As I choose the flash active mode, it should be effective after power on next time. But it won't work.

I use the jtag to connect the device and check the flash memory, the data is retained in the right address.

The develop enviornment is CCS V5.5.0 and the F28M35x Control Card with the core F28M35H52C1.

Map file:

OUTPUT FILE NAME:   <blinky_dc_m3.out>
ENTRY POINT SYMBOL: "_c_int00"  address: 00205431


MEMORY CONFIGURATION

         name            origin    length      used     unused   attr    fill
----------------------  --------  ---------  --------  --------  ----  --------
  CSM_ECSL_Z1           00200000   00000024  00000000  00000024  RWIX
  CSM_RSVD_Z1           00200024   0000000c  00000000  0000000c  RWIX
  RESETISR              00200030   00000008  00000006  00000002  R  X
  INTVECS               00201000   000001b0  000001b0  00000000  R  X
  FLASHLOAD             00201200   00002e00  000000bc  00002d44  R  X
  FLASH1                00204000   0001c000  0000160a  0001a9f6  R  X
  FLASH2                00260000   0001ff00  00000000  0001ff00  R  X
  CSM_RSVD_Z2           0027ff00   000000dc  00000000  000000dc  RWIX
  CSM_ECSL_Z2           0027ffdc   00000024  00000000  00000024  RWIX
  C0                    20000000   00002000  0000036c  00001c94  RW X
  C1                    20002000   00002000  00000000  00002000  RW X
  BOOT_RSVD             20004000   00000900  00000000  00000900  R  X
  C2                    20004900   00001700  00000014  000016ec  RW X
  C3                    20006000   00002000  00000000  00002000  RW X
  CTOMRAM               2007f000   00000800  00000000  00000800  R  X
  MTOCRAM               2007f800   00000800  00000000  00000800  RW X


SEGMENT ALLOCATION MAP

run origin  load origin   length   init length attrs members
----------  ----------- ---------- ----------- ----- -------
00200030    00200030    00000006   00000006    r-x
  00200030    00200030    00000006   00000006    r-x .resetisr
00201000    00201000    000001b0   000001b0    r--
  00201000    00201000    000001b0   000001b0    r-- .intvecs
00204000    00204000    00001610   00001610    r-x
  00204000    00204000    000014ce   000014ce    r-x .text
  002054d0    002054d0    00000104   00000104    r-- .const
  002055d8    002055d8    00000038   00000038    r-- .cinit
20000000    00201200    000000bc   000000bc    r-x
  20000000    00201200    000000bc   000000bc    r-x ramfuncs
200000bc    200000bc    00000100   00000000    rw-
  200000bc    200000bc    00000100   00000000    rw- .stack
20000400    20000400    000001b0   00000000    rw-
  20000400    20000400    000001b0   00000000    rw- .vtable
20004900    20004900    00000014   00000000    rw-
  20004900    20004900    00000014   00000000    rw- .data