Other Parts Discussed in Thread: TM4C123GH6PM
I am trying to interface ultrasonic sensor HC-SR04 with tiva c and i am having a problem with the IntEnable in my code,what could i be doing wrong
Description Resource Path Location Type
#20 identifier "INT_GPIOD_" is undefined sonar_master.c /sona_master line 43 C/C++ Problem
Description Resource Path Location Type
#20 identifier "INT_TIMER0A_" is undefined sonar_master.c /sona_master line 55 C/C++ Problem
here is the full code
/*
* main.c
*/
#include <stdint.h>
#include <stdbool.h>
#include <time.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "inc/hw_ints.h"
#include "driverlib/interrupt.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/timer.h"
#include "driverlib/pin_map.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#define SONAR_PORT GPIO_PORTD_BASE
#define TRIG_PIN GPIO_PIN_1
#define ECHO_PIN GPIO_PIN_0
#define SERVO_PIN GPIO_PIN_2
unsigned long f_cpu = 0;
unsigned long dist = 0;
void hw_init(void){
SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
f_cpu = SysCtlClockGet();
SysTickPeriodSet(0xffffffff);
SysTickEnable();
// UARTStdioInit();
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
GPIODirModeSet(SONAR_PORT, TRIG_PIN, GPIO_DIR_MODE_OUT);
GPIODirModeSet(SONAR_PORT, SERVO_PIN, GPIO_DIR_MODE_OUT);
GPIOPinTypeGPIOInput(SONAR_PORT, ECHO_PIN);
GPIOIntTypeSet(SONAR_PORT, ECHO_PIN, GPIO_RISING_EDGE);
GPIOPinIntEnable(SONAR_PORT,ECHO_PIN);
IntEnable(INT_GPIOD);
//Timer configuration
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
TimerConfigure(TIMER0_BASE, TIMER_CFG_A_PERIODIC);
const long timer_match = (f_cpu/1000000)*10;
const long timer_out = (f_cpu/1000)*80;
TimerLoadSet(TIMER0_BASE, TIMER_A, timer_out);
TimerMatchSet(TIMER0_BASE, TIMER_A, timer_match);
TimerEnable(TIMER0_BASE, TIMER_A);
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
TimerIntClear(TIMER0_BASE,TIMER_A);
IntEnable(INT_TIMER0A);
IntMasterEnable();
}
void main(void) {
hw_init();
while(1){
}
}
void Timer0AIntHandler(void){
static char flag = 0;
if(flag){
GPIOPinWrite(SONAR_PORT,TRIG_PIN,0);
TimerIntDisable(TIMER0_BASE, TIMER_TIMA_MATCH);
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
flag = 0;
}else{
GPIOPinWrite(SONAR_PORT,TRIG_PIN,1);
TimerIntDisable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_MATCH);
flag = 1;
}
}
void GPIODIntHandler(void){
static unsigned long cnt = 0;
static int state = 0;
if (state){
//dist = (f_cpu/(SysTickValueGet()-cnt))*58;
dist = SysTickValueGet();
dist = cnt - dist;
GPIOIntTypeSet(SONAR_PORT, ECHO_PIN, GPIO_RISING_EDGE);
state = 0;
}else{
cnt = SysTickValueGet();
GPIOIntTypeSet(SONAR_PORT, ECHO_PIN, GPIO_FALLING_EDGE);
state = 1;
}
}