This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding about Capture High Pulse.

Hi,

Can we use TimerValueGet () to obtain the HIGH pulse which act like arduino pulseIn()?

This is used for HC-SR04 Ultrasonic Sensor.

  • Hello 311Nice,

    The Timer only captures edges. A call of TimerValueGet will not give the High Pulse Width.

    To get the pulse width, you will have to set it rising edge capture. On Interrupt get the timer value and set it for falling edge. On second interrupt again get the Timer Value.and set it back to Rising edge for the next pulse.

    The difference of the two timer values will give you the pulse width

    Please do make sure that the Timer in Edge Time mode is a 16-bit timer so the events of rise and fall should happen within 2^16 system clocks. Otherwise pre scalar would be needed as well.

    Regards

    Amit

  • //initialise system
    void main(){
    
    	//configure oscillator & timer
    	SysCtlClockSet(SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN|SYSCTL_USE_PLL|SYSCTL_SYSDIV_5); //set timer to 40Mhz
    	SysCtlPeripheralEnable(echo_timer_en); //enable timer
    	TimerConfigure(echo_timer,echo_con); //configure timer
    	TimerPrescaleSet(echo_timer,TIMER_A,40); //adjust timer speed
    	TimerLoadSet(echo_timer,TIMER_A,65000); //set period
    	TimerDisable(echo_timer,TIMER_A); //disable clock
    
    	//configure pin
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF|sensor_port_en); //enable port e for sensor & port f for LED
    	GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, 0x0E); //configure led output
    	GPIOPinTypeGPIOOutput(sensor_port,trig_pin); //configure trig output
    
    	//configure interrupt
    	GPIOIntEnable(sensor_port, echo_pin); //configure echo as gpio interrupt
    	GPIOIntTypeSet(sensor_port, echo_pin, GPIO_BOTH_EDGES); //to detect both edges for echo to measure pulse
    	IntEnable(sensor_port); //enable int
    	IntMasterEnable();
    
    	while(1){
    
    		trigger();
    		//calculation
    			distance = (65000 - pulse)/58;
    		if (distance < 2){
    			GPIOPinWrite(GPIO_PORTF_BASE,0x0E,0x02);
    		}else {
    			GPIOPinWrite(GPIO_PORTF_BASE,0x0E,0x04);
    		}
    	}
    }
    
    //initialise trigger pin
    void trigger(){
    
    	//check echo status
    	if (checkecho ==0){
    		GPIOPinWrite(sensor_port,trig_pin,1); //set trig high
    		SysCtlDelay(trig_delay*SysCtlClockGet()/400); //delay 10us based on datasheet
    
    	}
    }
    
    //check echo pulse
    void GPIOEIntHandler(){
    
    	GPIOIntClear(sensor_port,echo_pin); //clear interrupt flag
    	echo = GPIOPinRead(sensor_port,echo_pin);
    	if (echo==1){
    
    		TimerEnable(echo_timer,TIMER_A); //start timer to record
    		checkecho = 1; //set checkecho 1 to prevent new trigger signal
    
    	}else{
    
    		TimerDisable(echo_timer,TIMER_A); //stop timer
    		pulse = TimerValueGet(echo_timer,TIMER_A); //record value
    	}
    }

    This is my testing code. Did I configure the timer coding correctly?

    Any mistake on it?

  • Hello 311Nice

    Yes, there are a few.

    1. GPIOPinRead on return will return the value in the Data Register. So the comparison has to be made as echo == echo_pin

    2. GPIOPinWrite for setting and clearing a pin has to be done

    GPIOPinWrite(sensor_port,trig_pin,trig_pin);
    GPIOPinWrite(sensor_port,trig_pin,~(trig_pin));

    3.What is the div by 58 factor for?

    4. IntEnable will not have the Port Address but the Port Interrupt

    5. SysCtlPeripheralEnable can accept only one peripheral at a time. Logical operations are prohibited.

    Regards

    Amit

  • Hi,

    The div by 58 is based on the formula that used to calculate distance.

    By the way, I unable to display the distance via UART. Is that any mistake on configuration on the Timer or GPIO ports?  

  • Hello 311Nice,

    The UART has to be initialized. That is not done in the code. Include the header file and the code below. After that UARTprintf should work.

    #include "utils/uartstdio.h"

    void
    InitConsole(void)
    {
        //
        // Enable GPIO port A which is used for UART0 pins.
        // TODO: change this to whichever GPIO port you are using.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

        //
        // Configure the pin muxing for UART0 functions on port A0 and A1.
        // This step is not necessary if your part does not support pin muxing.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinConfigure(GPIO_PA0_U0RX);
        GPIOPinConfigure(GPIO_PA1_U0TX);

        //
        // Enable UART0 so that we can configure the clock.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

        //
        // Use the internal 16MHz oscillator as the UART clock source.
        //
        UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);

        //
        // Select the alternate (UART) function for these pins.
        // TODO: change this to select the port/pin you are using.
        //
        GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

        //
        // Initialize the UART for console I/O.
        //
        UARTStdioConfig(0, 115200, 16000000);
    }

    Regards

    Amit

  • Oh, sorry to mention that I had configured on my another coding yet it does not showing any value at all.

  • Hello 311Nice,

    Can you please share the code so that I can give points on troubleshooting?

    Regards

    Amit

  • //initialise system
    void main(){
    
    	//configure oscillator & timer
    	SysCtlClockSet(SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN|SYSCTL_USE_PLL|SYSCTL_SYSDIV_5); //set timer to 40Mhz
    	SysCtlPeripheralEnable(echo_timer_en); //enable timer
    	TimerConfigure(echo_timer,echo_con); //configure timer
    	TimerPrescaleSet(echo_timer,TIMER_A,40); //adjust timer speed
    	TimerLoadSet(echo_timer,TIMER_A,65000); //set period
    	TimerDisable(echo_timer,TIMER_A); //disable clock
    
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    	GPIOPinConfigure(GPIO_PA0_U0RX);
    	GPIOPinConfigure(GPIO_PA1_U0TX);
    	GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    	UARTStdioConfig(0, 9600, SysCtlClockGet());
    
    	//configure pin
    	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); //enable port e for sensor & port f for LED
    	SysCtlPeripheralEnable(sensor_port_en);
    	GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, 0x0E); //configure led output
    	GPIOPinTypeGPIOOutput(sensor_port,trig_pin); //configure trig output
    	GPIOPinTypeGPIOInput(sensor_port,echo_pin); //configure echo input
    
    	//configure interrupt
    	GPIOIntEnable(sensr_port, echo_pin); //configure echo as gpio interrupt
    	GPIOIntTypeSet(sensor_port, echo_pin, GPIO_BOTH_EDGES); //to detect both edges for echo to measure pulse
    	IntEnable(IN_GPIOE); //enable int
    	IntMasterEnable();
    
    	while(1){
    
    		trigger();
    		//calculation
    			distance = (65000 - pulse)/58;
    		if (distance < 2){
    			GPIOPinWrite(GPIO_PORTF_BASE,0x0E,0x02);
    		}else {
    			GPIOPinWrite(GPIO_PORTF_BASE,0x0E,0x04);
    		}
    		UARTprintf("Hello I am Tiva C Series LaunchPad!\n",distance);
    	}
    }
    
    //initialise trigger pin
    void trigger(){
    
    	//check echo status
    	if (checkecho ==0){
    		GPIOPinWrite(sensor_port,trig_pin,trig_pin); //set trig high
    		SysCtlDelay(trig_delay*SysCtlClockGet()/60); //delay 10us based on datasheet
    	
    	}
    }
    
    //check echo pulse
    void GPIOEIntHandler(){
    
    	GPIOIntClear(sensor_port,echo_pin); //clear interrupt flag
    	echo = GPIOPinRead(sensor_port,echo_pin);
    	if (echo==echo_pin){
    
    		TimerEnable(echo_timer,TIMER_A); //start timer to record
    		checkecho = 1; //set checkecho 1 to prevent new trigger signal
    
    	}else{
    
    		TimerDisable(echo_timer,TIMER_A); //stop timer
    		pulse = TimerValueGet(echo_timer,TIMER_A); //record value
    
    	}
    }

    Here you go.

  • Hello 311Nice,

    You need to add %d as shown below.

    UARTprintf("Hello I am Tiva C Series LaunchPad! %d\n",distance);

    Also you are using Baud Rate of 9600. Please make sure that device manager of the PC and the Terminal application are also configured for 9600.

    Regards

    Amit

  • Ok. Noted.

    By the way, can you help me to check the configuration for pulse width capturing timer and gpio setup.

    I'm trying to emulate the function pulseIn from arduino.

    Thank You.

  • Hello 311Nice,

    I am not sure of Arduino setup to emulate it. But if the pulseIn is coming from Arduino, then you may want to make sure that the trigger function is over before the Input Pulse comes in, otherwise there may be some problem with the timing calculated.

    Regards

    Amit

  • What does the " trigger function is over before the Input Pulse comes in" means by?

  • Hello 311Nice,

    The trigger function is in a while loop and it keeps on executing and it could be possible the trigger and the input pulse at some point may come together and messing up the computation.

    Basically after the trigger do make sure you wait for the interrupt to fire before doing anything else.

    Regards

    Amit