Other Parts Discussed in Thread: LMFLASHPROGRAMMER
Hello,
I am trying to debug my code but every time I launch the debuggging session in CCS it doesn't pause at the start of the main function but instead when I hit pause it shows that I am already in the FaultISR. I can see the global variables that I set before the main program but not any of the variables that I set inside the main function.
I have attached my code. Please help me figure out how to get the debugger to run until the start of the main function.
Regards,
Curtis
/*
* GTBE_pllTest.c
*/
//Define Inputs\
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_ssi.h"
#include "inc/hw_types.h"
#include "inc/hw_ints.h"
// Stellarisware
#include "driverlib/sysctl.h"
#include "driverlib/rom.h"
#include "driverlib/debug.h"
#include "driverlib/flash.h"
// CMSIS
#include <math.h>
#include "arm_math.h"
#include "math_helper.h"
// PLL Loop Parameters
#define PHASE_OFFSET 0.0
#define F_C 10000 // Center Frequency of the NCO
// Test Input data
//#define NUM_CYCLES 1000
#define F_S 100000
#define A 100000
#define F_IN 10100
#define K_GAIN -0.01
#define NUM_SAMPLES 2000
//FIR Filter Data
#define NUM_TAPS 121
#define BLOCK_SIZE 1
#ifndef M_PI
#define M_PI 3.14159265358979323846
#endif
/*******************
* Flash Functions *
*******************/
/**
* Initializes the Flash
* Protects the part of the flash memory from address codeStart through
* codeStart + codeReserveLength by setting to only execute (FlashExecuteOnly)
* Sets up the flash interrupt in case the program attempts to access the
* protected flash portions. Make sure the ISR is added to the NVIC table
*
* \param codeStart - start location of flash memory that is to be reserved
* it must land on a 2KB boundry
* \param codeReserveLength - length of code to prtotect in flash memory
* it must land on a 2KB boundry
**/
void initFlash(uint32_t codeStart, uint32_t codeReserveLength) {
int32_t status;
uint32_t modCheck;
uint32_t block;
// Check codeStart and codeReserveLength to ensure the protected memory
// block starts and ends on a 2KB boundry
modCheck = codeStart - codeStart/0x800;
modCheck = modCheck + codeReserveLength/0x800;
ASSERT(modCheck == 0);
// Setup code protection
for(block = 0; block < (codeReserveLength/0x800); block++) {
status = FlashProtectSet(0x800 * block, FlashExecuteOnly);
ASSERT(status == 0)
}
//setup Flash Interrupt to handle any improper write attempts to flash
FlashIntEnable(FLASH_INT_PROGRAM);
}
/**
* Interrupt handler (ISR) that executes when an improper write to flash is attempted
**/
void FLASH_badWriteISR(void) {
while(1) {
// Do nothing - save state for examination
}
}
/******************
* FPU Functions *
******************/
/**
* Initializes the FPU
**/
void setupFPU(void) {
// Lazy Stacking increases interrupt latency and stack usage
// (only need if doing floating pt. in interrupts)
//FPULazyStackingEnable();
ROM_FPUEnable();
}
// Input
float32_t g_sig_I[NUM_SAMPLES];
// PFD
float32_t g_msig_I[1];
uint32_t gp_msig_I = 0x2800; // Address to save data to in flash
float32_t g_msig_Q[1];
uint32_t gp_msig_Q = 0x3600; // Address to save data to in flash
// FIR Filter
uint32_t blockSize = BLOCK_SIZE;
const float32_t firCoeffs32[NUM_TAPS] = {
0.0006830547454, 0.0007069055674, 0.0007422978673, 0.000790029838, 0.0008508535077, 0.0009254696142, 0.001014522694, 0.001118596418, 0.001238209203, 0.001373810118, 0.001525775132,
0.001694403697, 0.001879915716, 0.002082448903, 0.002302056559, 0.002538705765, 0.002792276037, 0.003062558419, 0.003349255047, 0.00365197918, 0.003970255708, 0.00430352213,
0.00465113001, 0.005012346894, 0.0053863587, 0.005772272552, 0.006169120058, 0.006575861016, 0.006991387523, 0.00741452848, 0.007844054463, 0.008278682938, 0.008717083793,
0.009157885164, 0.00959967952, 0.01004102998, 0.01048047682, 0.01091654416, 0.01134774676, 0.01177259695, 0.01218961154, 0.01259731883, 0.01299426559, 0.01337902392,
0.01375019813, 0.01410643139, 0.01444641227, 0.0147688811, 0.01507263604, 0.01535653896, 0.01561952094, 0.01586058754, 0.01607882362, 0.01627339785, 0.01644356679,
0.01658867855, 0.01670817598, 0.01680159946, 0.0168685891, 0.01690888657, 0.01692233637, 0.01690888657, 0.0168685891, 0.01680159946, 0.01670817598, 0.01658867855,
0.01644356679, 0.01627339785, 0.01607882362, 0.01586058754, 0.01561952094, 0.01535653896, 0.01507263604, 0.0147688811, 0.01444641227, 0.01410643139, 0.01375019813,
0.01337902392, 0.01299426559, 0.01259731883, 0.01218961154, 0.01177259695, 0.01134774676, 0.01091654416, 0.01048047682, 0.01004102998, 0.00959967952, 0.009157885164,
0.008717083793, 0.008278682938, 0.007844054463, 0.00741452848, 0.006991387523, 0.006575861016, 0.006169120058, 0.005772272552, 0.0053863587, 0.005012346894, 0.00465113001,
0.00430352213, 0.003970255708, 0.00365197918, 0.003349255047, 0.003062558419, 0.002792276037, 0.002538705765, 0.002302056559, 0.002082448903, 0.001879915716, 0.001694403697,
0.001525775132, 0.001373810118, 0.001238209203, 0.001118596418, 0.001014522694, 0.0009254696142, 0.0008508535077, 0.000790029838, 0.0007422978673, 0.0007069055674, 0.0006830547454
};
static float32_t firStateF32_I[BLOCK_SIZE + NUM_TAPS - 1]; //Declare State buffer of size (numTaps + blockSize - 1)
static float32_t firStateF32_Q[BLOCK_SIZE + NUM_TAPS - 1];
static float32_t I_err[1]; //output of I FIR filter
static float32_t Q_err[1]; //output of Q FIR filter
// Loop Gain and phase offsets
float32_t g_err[1];
uint32_t gp_err = 0x4400; // Address to save data to in flash
float32_t g_errAdj;
float32_t g_K = K_GAIN;
float32_t g_phaseOffset = PHASE_OFFSET;
// NCO
float32_t g_currPhase[NUM_SAMPLES];
uint32_t gp_currPhase;
float32_t g_nco_I[1];
float32_t g_nco_Q[1];
uint32_t gp_nco_I;
uint32_t gp_nco_Q;
/********
* Main *
********/
int main(void) {
int i;
// FIR Filter Variables
arm_fir_instance_f32 S_I;
arm_fir_instance_f32 S_Q;
float32_t *inputF32_I, *outputF32_I;
float32_t *inputF32_Q, *outputF32_Q;
//Initialize input and output buffer pointers
inputF32_I = &g_msig_I[0];
outputF32_I = &I_err[0];
inputF32_Q = &g_msig_Q[0];
outputF32_Q = &Q_err[0];
// NCO
float32_t phaseInc;
//
// System Initialization
//
// Set system clock to 80 MHz (400MHz main PLL (divided by 5 - uses DIV400 bit) [16MHz external xtal drives PLL]
ROM_SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
setupFPU();
initFlash(0x0, 0x2800);
// Initialize FIR Filter
/* Call FIR init function to initialize the instance structure. */
arm_fir_init_f32(&S_I, NUM_TAPS, (float32_t *)&firCoeffs32[0], &firStateF32_I[0], blockSize);
arm_fir_init_f32(&S_Q, NUM_TAPS, (float32_t *)&firCoeffs32[0], &firStateF32_Q[0], blockSize);
//
// Generate Test Input cosine
//
for(i=0; i<NUM_SAMPLES; i++) {
g_sig_I[i] = arm_cos_f32((2 * M_PI * F_IN / F_S) *i);
}
phaseInc = (2 * M_PI * F_C)/F_S;
g_nco_I[0] = 1;
g_nco_Q[0] = 0;
FlashProgram(g_nco_I,gp_nco_I,4);
gp_nco_I += 4;
FlashProgram(g_nco_Q,gp_nco_Q,4);
gp_nco_Q += 4;
int n;
// Main "Time" sim loop
for(n = 0; n < NUM_SAMPLES; n++) {
//
// Phase Detection
//
// PD Multipliers
g_msig_I[0] = g_sig_I[n] * g_nco_I[0];
g_msig_Q[0] = g_sig_I[n] * g_nco_Q[0];
FlashProgram(g_msig_I,gp_msig_I,4);
gp_msig_I += 4;
FlashProgram(g_msig_Q,gp_msig_Q,4);
gp_msig_Q += 4;
// PD FIR Filter
arm_fir_f32(&S_I, inputF32_I, outputF32_I, blockSize);
arm_fir_f32(&S_Q, inputF32_Q, outputF32_Q, blockSize);
g_err[0] = atan2(Q_err[0],I_err[0]); // Take the 4 quadrant arctan
FlashProgram(g_err,gp_err,4);
gp_err += 4;
g_errAdj = g_K * (g_err[0] + g_phaseOffset);
if(n>0) g_currPhase[n] = g_currPhase[n] + phaseInc + g_errAdj;
else g_currPhase[0] = 0;
g_nco_I[0] = arm_cos_f32(g_currPhase[n]);
g_nco_Q[0] = arm_sin_f32(g_currPhase[n]);
FlashProgram(g_nco_I, gp_nco_I, 4);
FlashProgram(g_nco_Q, gp_nco_Q, 4);
}
while(1) {} // End of program execution
}