This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129XL Connected Launchpad: temp calibration

I just received my Connected Launchpad and I'm using the examples to round out my knowledge. I've also studied the CPU datasheet at length.

The formula in the CPU datasheet to convert the Temp Sensor reading to Celsius is TEMP = 147.5 - ((75 * (VREFP - VREFN) × ADCCODE) / 4096)  (sec. 15.3.6 pg. 1062).

Using VREFP=3.3V and VREFN=0V I get 147.5 - 75*3.3*ADCCODE/4096

By oversampling I can easily get a value with 12 bits apparent precision but the calibration appears to be off. I'm using a digital thermometer applied to the CPU package and reading room temperature but I'm receiving ADCCODE=0x7c2 which I interpret as 27.4963 C.

After googling for a while I decided to create an account and ask here: is this device temp-calibrated?