Hello,
i am using I am using 123GH6PGE DK , TivaWare_C_Series-1.1 ,CCS 5.4 and tirtos_1_21_00_09
1-If i want to use the free area of the flash for my data storage i know that i can determine the range where to load my program by CCS's CMD file and i can retrieve the unused data from the map file ,but what should i do to retrieve this amount of Free(Unused) area dynamically.
2-When i try to write to the code area on flash (after erasing it) i don't get any error indication and it lets me program over the code data