Other Parts Discussed in Thread: SYSBIOS
Hello,
i am using I am using 123GH6PGE DK , TivaWare_C_Series-1.1 ,CCS 5.4 and tirtos_1_21_00_09
i am trying to program flash using Tivaware APIs and create sysbios -Managed ISR through that main file but the problem is that while i am trying to run that application the bios always start with the hwi ISR and when it comes to the task it doesn't triggers an interrupt when erasing or writing
//---------------------------------------------------------------------------
// Project: Flash Sample1
// Author: AHmed Hassan
// Date: March 2014
//---------------------------------------------------------------------------
/*
* This Sample is to provide safe thread operation
*
*/
//------------------------------------------
// TivaWare Header Files
//------------------------------------------
#include <stdint.h>
#include <stdbool.h>
#include<stdio.h>
#include "driverlib/flash.h"
#include "driverlib/sysctl.h"
#include "driverlib/interrupt.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
//----------------------------------------
// BIOS header files
//----------------------------------------
#include <xdc/std.h> //mandatory - have to include first, for BIOS types
#include <ti/sysbios/BIOS.h> //mandatory - if you call APIs like BIOS_start()
#include <xdc/runtime/Log.h> //needed for any Log_info() call
#include <xdc/cfg/global.h> //header file for statically defined objects/handles
#include <xdc/std.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Timestamp.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/hal/Timer.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/knl/Swi.h>
#include "inc/hw_ints.h"
#define int_ID 45 /*defining Flash Memory Control vector number */
/*Function Prototype */
void Flash_Writing(void);
void Flash_ISR(void);
void Flash_led(void);
void hardware_init(void);
Error_Block eb;
/*create HWI */
Hwi_Handle hwi0;
Hwi_Params hwiParams;
/* Create SWI */
Swi_Handle LEDSwi;
Swi_Params swiParams;
/*Task */
Task_Params taskParams;
Task_Handle myTsk;
void Flash_ISR(void)
{
Hwi_disableInterrupt(int_ID);
Swi_post(LEDSwi); // post LEDSwi
}
void Flash_led(void)
{
GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_2, 0x04);
SysCtlDelay(2000000);
GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_2, 0x00);
}
void hardware_init(void)
{
/* Enable the GPIO PortG Peripheral*/
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
/* Make PIN 2 as Output Pin*/
GPIOPinTypeGPIOOutput(GPIO_PORTG_BASE,GPIO_PIN_2);
GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_2, 0x00);
}
void Flash_Writing(void)
{
uint32_t pui32Data[2];
pui32Data[0] = 0x12345678;
pui32Data[1] = 0x56789abc;
uint32_t ui32User0_Set=0XEEEEEEEE; /*the value to be written to user register 0 */
uint32_t ui32User1_Set=0XDDDDDDDD; /*the value to be written to user register 1 */
int8_t FRESULT; /*To check the success of the programming*/
FRESULT=-1;
uint32_t ui32User0_Get;
uint32_t ui32User1_Get;
/* ERASE A BLOCK AT FLASH*/
FRESULT=FlashErase(0x20000);
if(FRESULT==-1)
{
printf("error erasing");
}
/* Program some data into the newly erased block of the flash*/
FRESULT=FlashProgram(pui32Data,0x20000, sizeof(pui32Data));
if(FRESULT==-1)
{
printf("error programming");
}
/*sets the contents of the user registers (0 and 1)*/
FlashUserSet(ui32User0_Set,ui32User1_Set);
/*reads the contents of user registers (0 and 1), and stores them */
FlashUserGet(&ui32User0_Get,&ui32User1_Get);
}
/*
* main.c
*/
void main()
{
/*HW INtialization*/
hardware_init();
/* Initialize error block and hwiParams to default values */
Error_init(&eb);
Hwi_Params_init(&hwiParams);
hwi0 = Hwi_create(int_ID,Flash_ISR, &hwiParams, &eb);
/* Set Flash_ISR parameters */
// hwiParams.arg = 12;
hwiParams.enableInt = FALSE; /* override default setting: Keep interrupt disabled until later */
// don't allow this interrupt to nest itself
hwiParams.maskSetting = Hwi_MaskingOption_SELF;
if (hwi0 == NULL) {
System_abort("Hwi create failed");
}
/* Initialize swiParams to default values */
Swi_Params_init(&swiParams);
LEDSwi = Swi_create(Flash_led, &swiParams, &eb);
swiParams.priority = 10;
if (LEDSwi == NULL) {
System_abort("Swi create failed");
}
/*Initialize taskParams to default values */
Task_Params_init(&taskParams);
taskParams.stackSize = 512;
taskParams.priority = 3;
myTsk = Task_create((Task_FuncPtr)Flash_Writing, &taskParams, &eb);
if (myTsk == NULL) {
System_abort("hiPriTask create failed");
}
/* enable interrupts */
Hwi_enableInterrupt(int_ID);
FlashIntEnable(FLASH_INT_PROGRAM);
Hwi_enable();
/* start BIOS */
BIOS_start();
}
Regards,
Ahmed