Hi,
For the GIO of TMS5703137CGWTQEP, Pin N17 (EMIF_NCS0_RTP_DATA15_N2HET2_7), output drive strength is specified as 8mA in Table 3-2 of datasheet.
1. What is the maximum capacitive load it can drive?
2. Is this GIO pin strong enough to drive the complementary PMOS, NMOS pair (Inverting Push-Pull stage) comprised of Si2302CDS (Ciss=320pF) & Si2323CDS (Ciss=1200pF)?
3. Can you explain the characteristics of this GIO drive stage? Is it a voltage source that is current limited?
4. What is the peak safe current that can be drawn from this pin?
5. What is the output resistance of this pin?
Thanks,
Shihab.