I'm having issues with the basic functions of my CC3000BOOST. I tried using the Energia software library for programming the EK-TM4C123GXL and the basic programs work (BLINK, FADE etc) but when I try to test wireless (with the simplewebserver example) I never get any response signifying connectivity and the website is not accessible. The sample code is posted beneath. I'm thinking software issue but am open to other suggestions for troubleshooting.
// Enter here the name (=SSID) and password of your WiFi LAN
#define WLAN_SSID "energia" // cannot be longer than 32 characters!
#define WLAN_PASS "supersecret"
/*
Web Server
A simple web server that shows the value of the analog and digital input pins
using a WiFi BoosterPack.
This example is written for a network using WPA encryption. For
WEP or WPA, change the Wifi.begin() call accordingly.
Circuit:
* WiFi BoosterPack
Created: October 16, 2013 by Robert Wessels (http://energia.nu)
Derived from example Sketch by Hans Scharler (http://www.iamshadowlord.com)
*/
#include "SPI.h"
#include "WiFi.h"
// Prototypes
void printConfig();
void printWifiData();
void printIndex();
void printHelp();
char ssid[] = WLAN_SSID; // your network SSID (name)
char pass[] = WLAN_PASS; // your network SSID (name)
WiFiServer server(80);
WiFiClient client;
int statusConfig = 0;
void setup() {
Serial.begin(115200);
// Set communication pins for CC3000
WiFi.setCSpin(18); // 18: P2_2 @ F5529, PE_0 @ LM4F/TM4C
WiFi.setENpin(2); // 2: P6_5 @ F5529, PB_5 @ LM4F/TM4C
WiFi.setIRQpin(19); // 19: P2_0 @ F5529, PB_2 @ LM4F/TM4C
pinMode(RED_LED, OUTPUT);
pinMode(GREEN_LED, OUTPUT);
pinMode(PUSH1, INPUT_PULLUP); // released = HIGH, pressed = LOW
pinMode(PUSH2, INPUT_PULLUP);
delay(10);
// Connect to an AP with WPA/WPA2 security
Serial.println("Connecting to WiFi....");
WiFi.begin(ssid, pass);
//WiFi.begin(ssid);
server.begin();
Serial.println("Connect success!");
Serial.println("Waiting for DHCP address");
// Wait for DHCP address
delay(5000);
// Print WiFi status and DHCP address
// To print the status and DHCP info again, type "i" in the Serial monitor and press send.
printWifiData();
}
void loop() {
client = server.available();
if (client) { // if you get a client,
Serial.println("new client"); // print a message out the serial port
String currentLine = ""; // make a String to hold incoming data from the client
while (client.connected()) { // loop while the client's connected
if (client.available()) { // if there's bytes to read from the client,
char c = client.read(); // read a byte, then
// This lockup is because the recv function is blocking.
Serial.print(c);
if (c == '\n') { // if the byte is a newline character
// if the current line is blank, you got two newline characters in a row.
// that's the end of the client HTTP request, so send a response:
if (currentLine.length() == 0) {
break;
}
else { // if you got a newline, then clear currentLine:
currentLine = "";
}
}
else if (c != '\r') { // if you got anything else but a carriage return character,
currentLine += c; // add it to the end of the currentLine
}
if (currentLine.endsWith("GET / ")) {
statusConfig = 0;
printIndex();
}
if (currentLine.endsWith("GET /config.html ")) {
statusConfig = 1;
printConfig();
}
if (currentLine.endsWith("GET /index.html ")) {
statusConfig = 0;
printIndex();
}
// Check to see if the client request was "GET /H" or "GET /L":
if (currentLine.endsWith("GET /RED_LED_H")) {digitalWrite(RED_LED, HIGH);printConfig();}
if (currentLine.endsWith("GET /RED_LED_L")) {digitalWrite(RED_LED, LOW);printConfig();}
if (currentLine.endsWith("GET /GREEN_LED_H")) {digitalWrite(GREEN_LED, HIGH);printConfig();}
if (currentLine.endsWith("GET /GREEN_LED_L")) {digitalWrite(GREEN_LED, LOW);printConfig();}
}
}
// close the connection:
client.stop();
Serial.println("client disonnected");
}
}
void printIndex()
{
// HTTP headers always start with a response code (e.g. HTTP/1.1 200 OK)
// and a content-type so the client knows what's coming, then a blank line:
client.println("HTTP/1.1 200 OK");
client.println("Content-type:text/html");
client.println();
client.println("<html><head><title>CC3000 Energia Webpage</title></head><body align=center>");
client.println("<h1 align=center><font color=\"red\">Welcome To CC3000 Web Server</font></h1>");
client.println("</br><font size=\"4px\"><table border=\"0\" align=center width=1200px height=590px>");
client.println("<tr><td align=center width=375></td><td width=450px align=left valign=\"top\">");
client.println("<p>Using CC3000 WLAN connectivity, Web Server provides ");
client.println("capability to remotely read and write GPIOs ");
client.println("on/off.</p></br></br>");
client.println("<p><a href=\"/config.html\">Click here</a> ");
client.println("to check status and configure the board</p>");
client.println("<td align=cneter width=375></td></tr></table></font></body></html>");
client.println();
}
void printConfig()
{
// HTTP headers always start with a response code (e.g. HTTP/1.1 200 OK)
// and a content-type so the client knows what's coming, then a blank line:
client.println("HTTP/1.1 200 OK");
client.println("Content-type:text/html");
client.println();
client.println("<html><head><title>CC3000 Energia Webpage</title></head><body align=center>");
client.println("<h1 align=center><font color=\"red\">Welcome To CC3000 Web Server</font></h1>");
// the content of the HTTP response follows the header:
// Added: nicer buttons
client.print("<font color='green'>GREEN_LED</font> <button onclick=\"location.href='/GREEN_LED_H'\">HIGH</button>");
client.println(" <button onclick=\"location.href='/GREEN_LED_L'\">LOW</button><br>");
client.print("<font color='red'>RED_LED</font> <button onclick=\"location.href='/RED_LED_H'\">HIGH</button>");
client.println(" <button onclick=\"location.href='/RED_LED_L'\">LOW</button><br><br>");
client.println("PUSH1 ");
if(digitalRead(PUSH1))client.print("is HIGH<br>");
else client.print("is LOW<br>");
client.println("PUSH2 ");
if(digitalRead(PUSH2))client.print("is HIGH<br>");
else client.print("is LOW<br>");
client.println("<a href=\"/config.html\" >refresh</a> <br>");
client.println("<a href=\"/index.html\" >home</a> <br>");
client.println("</body></html>");
// The HTTP response ends with another blank line:
client.println();
// break out of the while loop:
}
void serialEvent() {
while (Serial.available()) {
// get the new byte:
char inChar = (char)Serial.read();
switch(inChar) {
case 'h':
printHelp();
break;
case 'i':
printWifiData();
break;
default:
Serial.println();
Serial.println("Invalid menu option");
}
}
}
void printHelp() {
Serial.println();
Serial.println("+++++++++++++++++++++++++++++++++++++");
Serial.println("Help menu:");
Serial.println("\th: This help menu");
Serial.println("\ti: IP address information");
Serial.println("+++++++++++++++++++++++++++++++++++++");
}
void printHex(int num, int precision) {
char tmp[16];
char format[128];
sprintf(format, "%%.%dX", precision);
sprintf(tmp, format, num);
Serial.print(tmp);
}
void printWifiData() {
// print your WiFi shield's IP address:
Serial.println();
Serial.println("IP Address Information:");
IPAddress ip = WiFi.localIP();
Serial.print("IP Address: ");
Serial.println(ip);
// print your MAC address:
byte mac[6];
WiFi.macAddress(mac);
Serial.print("MAC address: ");
printHex(mac[5], 2);
Serial.print(":");
printHex(mac[4], 2);
Serial.print(":");
printHex(mac[3], 2);
Serial.print(":");
printHex(mac[2], 2);
Serial.print(":");
printHex(mac[1], 2);
Serial.print(":");
printHex(mac[0], 2);
Serial.println();
uint8_t *ver = WiFi.firmwareVersion();
Serial.print("Version: ");
Serial.print(ver[0]);
Serial.print(".");
Serial.println(ver[1]);
// print your subnet mask:
IPAddress subnet = WiFi.subnetMask();
Serial.print("NetMask: ");
Serial.println(subnet);
// print your gateway address:
IPAddress gateway = WiFi.gatewayIP();
Serial.print("Gateway: ");
Serial.println(gateway);
Serial.print("SSID: ");
Serial.println(WiFi.SSID());
IPAddress hostIp;
uint8_t ret = WiFi.hostByName("google.com", hostIp);
Serial.print("ret: ");
Serial.println(ret);
Serial.print("Google IP: ");
Serial.println(hostIp);
}