hi ,
1. I i am using TM4C1237H6PZ controller i configured it with 66.67MHz freq
SysCtlClockSet(SYSCTL_SYSDIV_3 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);;
I configured SSI at 33MHz
SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_3,SSI_MODE_MASTER, 33000000, 8);
It is working fine.
2. Now r i configured contoler with 80MHz freq
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);;
I configured SSI at 33MHz
SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_3,SSI_MODE_MASTER, 33000000, 8);
It is NOT WORKING .In this case SSI work only at 20MHz .
I tried above case with 25MHz crystal frequency,but i am facing the same problem. Why ??
Thanks & regards,
Dhanush