Other Parts Discussed in Thread: DRV8301, TMS570LS1227
Hi,
I started using the DRV8301 LS12 EVM kit.
I have run the GUI solution given in the kit for sensored FOC of BLDC , the motor works fine.
Then I installed CCS5.5 and try running the project "TMS570LS1227_sensored_speed_smo" .
I just followed steps in document "foc_encoder_speed_ls12" ( Sensored FOC Control with SMO for the
Hercules TMS570LS12)
Below are steps I followed
1. DIP SW1 all switched ff.
2. Build the code in ccs5 and use Run->debug to load the code.
3. disconnect from ccs5 and switched off power supply.
4. switches 1 &4 of DIP SW1 is switched ON for enabling TPS. (this is as per the above mentioned document for FOC control, but in the document for control card 570LS12 the dip switch 5 is for TPS enabling,)
5. Then powered up the kit and connect the targe in ccs5 environment. I got the below error
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0IcePick: Trouble Reading Memory Block at 0x0 on Page 0 of Length 0xc8
6. I tried calibrating , but the motor is not rotating for calibration purpose.
Could you please provide me solution, is it due to that wrong dip switch or any other problem?
Thanks & Regards,
Rathinavel