This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI Interface with TM4C123GH6PM

Hello,

I have started working on TM4C123GH6PM in SPI mode. I have also referred spi_master code provided in example but I am still unable to transmit my data from my controller to slave.Data I want to send consists of 8 bit,16 bit and 32 bit data. SO if anyone can suggest me with proper example and with connection. To make a proper interface.

This is the basic code I have written. Using this code I am getting data on UART but unable to transmit.

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_ssi.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/ssi.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"

uint32_t g_ui32Flags;

#ifdef DEBUG void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

void Timer0IntHandler(void)
{
char cOne, cTwo;
ROM_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
HWREGBITW(&g_ui32Flags, 0) ^= 1;
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, g_ui32Flags << 1);
ROM_IntMasterDisable();
cOne = HWREGBITW(&g_ui32Flags, 0) ? '1' : '0';
cTwo = HWREGBITW(&g_ui32Flags, 1) ? '1' : '0';
UARTprintf("\rT1: %c T2: %c", cOne, cTwo);
ROM_IntMasterEnable();
}

void Timer1IntHandler(void)
{
char cOne, cTwo;
ROM_TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
HWREGBITW(&g_ui32Flags, 1) ^= 1;
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, g_ui32Flags << 1);
ROM_IntMasterDisable();
cOne = HWREGBITW(&g_ui32Flags, 0) ? '1' : '0';
cTwo = HWREGBITW(&g_ui32Flags, 1) ? '1' : '0';
UARTprintf("\rT1: %c T2: %c", cOne, cTwo);
ROM_IntMasterEnable();
}

void ConfigureUART(void)
{
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
UARTStdioConfig(0, 9600, 16000000);
}

int main(void)
{
int n;
n=0x00;

uint32_t pui32DataTx[0];
uint32_t pui32DataRx[0];

SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);

ConfigureUART();

UARTprintf("start\n");

SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PA4_SSI0RX);
GPIOPinConfigure(GPIO_PA5_SSI0TX);

GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 | GPIO_PIN_2);

SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 1000000, 8);

// Enable the SSI0 module.
SSIEnable(SSI0_BASE);

while(SSIDataGetNonBlocking(SSI0_BASE, &pui32DataRx[0]))
{
}
while(1)
{
// Initialize the data to send.
pui32DataTx[0] = n;
UARTprintf("data: %d \n", pui32DataTx[0]);
SSIDataPut(SSI0_BASE, pui32DataTx[0]);
while(SSIBusy(SSI0_BASE))
{
}
n++;
}
}

Thank you,

Mitesh