Hi.
My question is regarding the TMS570LS3137.
In spnu499b.pdf, page 269 to 271, are the bit fields of register FEDACSTATUS described. Can you confirm that the Description of the following two bit fields are correct:
* ERR_ONE_FLG
* ERR_ZERO_ FLG
Two reasons for this question:
* Reason 1: In ERR_ONE_FLG is ONLY "bus 2" stated, but not "bus 1". But in ERR_ZERO_ FLG is "bus 1" and "bus 2" sated. Why this difference?
* Reason 2: In ERR_ZERO_ FLG is stated "This bit is set if ..., or if either the EZFEN or the EOFEN bits are set and any single bit error is detected and corrected on bus 1. ...". Why should an enabled EOFEN (Error on One Fail Enable) bit and a single bit error lead to setting of ERR_ZERO_ FLG (Error on Zero Fail Status Flag)?
Thank you and regards
Oliver.