This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC Sampling Interrupt



Hello,

 iam using CCS V 5.4 , 123GH6PGE DK ,Tivaware 2.1 and sysbios 6.63.1.24, and while i am trying to sample the internal temp. sensor reading Using Sample Sequencer 1 & Timer 0 trigger as a source of trigger. The problem is  that upon starting the debugging and without executing any statement in my application by checking the ADC register ADCIM ,ADCISC&ADCRIS i always find them initiated by 2 .which indicates as the ADC signal interrupt of sample sequencer 1 is sent to NVIC so i have to unpend that interrupt from NVIC to get the required behavior So,what i'd like to ask about is that why those status are set by default in initialization ?

Thanks

Regards

Ahmed