Other Parts Discussed in Thread: TMS570LS3137
Hi.
My questions are regarding the TMS570LS3137.
1. In spnu499b.pdf, page 269, is bit field FEDACSTATUS.ECC_B2_MAL_ERR described.
Question 1.1: Will this error generate also an ESM event (e.g. ESM group 1 channel 6 event)?
Question 1.2: In case no ESM event will be generated: What is your suggestion to work with this bit? I.e.: Should it be periodically be polled? Or will this bit always be set in combination with another bit of register FEDACSTATUS?
2. In spnu499b.pdf, page 300, is bit field EE_STATUS.EE_CMG described. BUT it's not described if this bit is only relevant for diagnostic mode. I assume that it's only relevant for diagnostic mode, cause the equivalent bit field for the main flash banks FEDACSTATUS.COMB2_MAL_G (see spnu499b.pdf, page 269) is only for diagnostic mode.
Question 2.1: Can you confirm my assumption?
3. In spnu499b.pdf, page 300, is bit field EE_STATUS.EE_CME stated.
Question 3.1: There is no description stated at all. But I assume that this bit field should have a similar description as the equivalent bit field for the main flash banks FEDACSTATUS.ECC_B2_MAL_ERR (see spnu499b.pdf, page 269). Is my assumption correct?
Question 3.2: Will this error generate also an ESM event (e.g. ESM group 1 channel 35 event)?
Question 3.3: In case no ESM event will be generated: What is your suggestion to work with this bit? I.e.: Should it be periodically be polled? Or will this bit always be set in combination with another bit of register EE_STATUS?
Thank you and regards
Oliver.