This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART error rate tiva

Expert 2355 points

Other Parts Discussed in Thread: TM4C1233H6PZ

Hi,

D/S describes that UART module decrease error to account for rounding errors.

Is there any other  error except for it ?

How do I think UART baudrate error in followed case?

------

Target device:tm4c1233h6pz

http://www.ti.com/product/tm4c1233h6pz

14.4 Initialization and Configuration

Baudrate:115,200bps

UARTsysclk: 20,000,000Hz

Div:16

------

best regards,

  • Hello Kyt,

    The 0.5 is added for any rounding error that arises in the fractional divisor after being multiplied by 64 when the fractional part is more than 0.5

    For the example mentioned, the Integer is 0xA and the Fractional is 54.44 before round off and 54.94 after round off. In this case the value to be programmed is 54 (decimal). Had it been 54.51 then the after round off it would 55.01 in which case the value to be programmed had to 55 (decimal)

    Regards

    Amit