Other Parts Discussed in Thread: TM4C129XNCZAD, EK-TM4C1294XL
Hi,
I have a DK-TM4C129X kit with a TM4C129XNCZAD processor. I am using Code Composer Studio, and set it up by following the instructions in spmu352.
I imported the enet_io example from the tivaware/examples/boards/dk-tm4c129x, and tried to build it. However, I get the following errors:
Description Resource Path Location Type This project was created using a version of compiler that is not currently installed: 5.0.4 [ARM]. Another version of the compiler will be used during build: 5.1.1. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. enet_io properties Problems unresolved symbol Kentec320x240x16_SSD2119Init, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol FrameDraw, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol LocatorInit, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol LocatorAppTitleSet, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol PinoutSet, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol LocatorMACAddrSet, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol http_set_cgi_handlers, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol g_sKentec320x240x16_SSD2119, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol httpd_init, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol http_set_ssi_handler, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol lwIPInit, first referenced in ./enet_io.obj enet_io C/C++ Problem unresolved symbol lwIPEthernetIntHandler, first referenced in ./startup_ccs.obj enet_io C/C++ Problem unresolved symbol usnprintf, first referenced in ./io.obj enet_io C/C++ Problem unresolved symbol lwIPTimer, first referenced in ./enet_io.obj enet_io C/C++ Problem #10234-D unresolved symbols remain enet_io C/C++ Problem #10010 errors encountered during linking; "enet_io.out" not built enet_io C/C++ Problem
I expected the example application (since it was written for this specific evaluation kit, after all) to run out of the box. What are causing the errors - did I mess up somewhere?
Thank you.