This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

generate the sound data file for Tiva C series board



Hi All,

I am using TM4C129x kit for my project.

Please let me know the solution for below issues.

1)      How to generate the sound data file for Tiva C series board.

2)      Reading & writing from Serial flash ram (MX66L51235F), when exciting the instruction  “MX66L51235FInit(ui32SysClock)“ for initialization of SPI3

Clock, system immidatly comes in FaultIsr(void).   

Kindly suggest !!

  • Had you earlier, "SysCtlPeripheralEnable()" SPI3?   Failure to do so always yields such fault.

  • 1)      Demo board connect with networking on DHCP  is random, it sometime get proper network IP & sometime not(default IP)

    Your suggestion to implement “Wiresark”  to check the network packages, but there are so many packages. Please suggest another good way.

     

    2)      We want to generate sound data file likes a) “ Thank You” b) “Put Finger Again” etc messages. 

    3)      Reading & writing from Serial flash ram (MX66L51235F), when exciting the instruction  “MX66L51235FInit(ui32SysClock)“ for initialization of SPI3

    Clock, system immidatly comes in FaultIsr(void).  

    5)      We want to use this MCU with LCD controller but it is difficult to us to handle boll type pins.  Is it available ready module on PCB with I/O pins or

    Available module with MCU & Color TFT LCD ?