This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

9BIT mode - read the address value

I have a TM4C123AH tiva processor.

I have configured the UART in 9-Bit Mode with interrupt

UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(), 38400,
                        (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
                         UART_CONFIG_PAR_ZERO));
    UARTFIFODisable (UART1_BASE);
    UARTIntEnable(UART1_BASE, UART_INT_RX | UART_INT_9BIT | UART_INT_FE);
UART_INT_FE | UART_INT_PE));
    UART9BitAddrSet(UART1_BASE, 0x83, 0xFF);        // slave address 03 fisso
    UART9BitEnable(UART1_BASE);
    IntEnable(INT_UART1);

When the interrupt routine is execute I cannot read the Address value
  ulStatus = UARTIntStatus(UART1_BASE, true);
  UARTIntClear(UART1_BASE, ulStatus);

  if (ulStatus & UART_MIS_9BITMIS)
    {
    while(UARTCharsAvail(UART1_BASE))
      {
      // NEVER ENTER HERE
      bufferRx[cntbufferRx] = UARTCharGet(UART1_BASE);
      cntbufferRx ++;
      }
    cntbufferRx = 0;
    }
   else  if (ulStatus & UART_MIS_RXMIS)
    {
    while(UARTCharsAvail(UART1_BASE))
      {
      bufferRx[cntbufferRx] = UARTCharGet(UART1_BASE);
      cntbufferRx ++;
      }
    }
}

Is it normal not read the data address in 9-BIT mode ?

Thanks