This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tiva C launchapad TM4C23GH6PM Power up program failure



I am using tica c launchpad TM4C123G6PM with CCS6 using TivaWare_C_Series-2.1.0.12573 to program it,i am having a problem with the power up program run,what i mean is i would program the tiva through the conected USB cable  and it will work just fine with the cable  connected but after disconnecting the tiva  and powering it up with something elde ot the USB cable itself  the code wont run,it lloks like it was not stored on the flash ,looks like ithe program was written to RAM.I tried everthng,using project0 that comes with tivaware examples,lab projects of the  launchpad workshop nothng seems to work.Its really frustrating to re-program the tiva while just changing a piece of line

How i'm i supposed to setup the environment? so i have a program just waiting inside flash to be powered up  and run accordingly with no need to re-install the program after swicth it off