HI,
Is it possible to use Tiva C connected TM4C1294XL for wireless application using CC3000EM?
What is the main difference between EK-TM4C123GXL and TM4C1294XL ?
Can we use TI_RTOS on this boards?
Regards,
Uma
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
Is it possible to use Tiva C connected TM4C1294XL for wireless application using CC3000EM?
What is the main difference between EK-TM4C123GXL and TM4C1294XL ?
Can we use TI_RTOS on this boards?
Regards,
Uma
Hi,
This post is more appropriate at the Tiva ARM Forum. As you can see above this webpage, that this is the MSP430 forum.
uma pv said:Is it possible to use Tiva C connected TM4C1294XL for wireless application using CC3000EM?
See, wiki below.
http://processors.wiki.ti.com/index.php/CC3000_Basic_Wi-Fi_example_application_for_Stellaris
uma pv said:What is the main difference between EK-TM4C123GXL and TM4C1294XL
You, can do a device datasheet compare.
Here is the Tiva ARM Forum below.
http://e2e.ti.com/support/microcontrollers/tiva_arm/default.aspx
-kel
Hi Uma,
Yes, TIVA ARM supports TI-RTOS.
Here, below mentioned in the link http://www.ti.com/tool/ti-rtos. TI ARM Cotex M4 is TIVA ARM.
"TI-RTOS Kernel is available on most TI microprocessors, microcontrollers and DSPs. TI-RTOS middleware and drivers and board initialization components are available on select ARM Cortex-M4, C2000™ dual core C28x + ARM Cortex-M3, and MSP430 microcontrollers. This support will be extended to additional microprocessor and DSP families in the future."
-kel
Hello Uma,
Both TM4C123 and TM4C129 support CC3000 Booster Pack and RTOS as well.
TM4C129 is the follow up device for TM4C123 and has more features (ethernet phy, more flash) and better performance. Of cousr you can go through the online product comparisons
Regard
Amit