This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Work EK-TM4C1294XL with BOOSTXL-DRV8301

Other Parts Discussed in Thread: EK-TM4C1294XL, BOOSTXL-DRV8301, CONTROLSUITE, DRV8301

I want to connect EK-TM4C1294XL to BOOSTXL-DRV8301 for BLDC-Control.

Which SW can I use.

I have downloaded both CCS and ControlSuite...

I m looking for someone with expiences with this connection...

I have found only Usergude for connection BOOSTXL-DRV8301 and a familly Piccolo (dsp..)

  • From a hardware perspective, the BOOSTXL-DRV8301 could be interfaced with EK-TM4C129XL. But at this point there is no software support.

    Having said that, the StellarisWare has some examples in the folder "boards/rdk-bldc" that you could use as a starting point to develop your own software. It can be downloaded from here.

    Note that StellarisWare supports the LM3S devices and the differences (with TivaWare) are described in this Migration document.

    Good Luck!

  • Thank You.

    I have downloaded the StallarisWare, and I will see, what I find.

    Q: The controling of DRV8301 in the mode (address 0x02)

    - PWM with three independent inputs. PWM control
    high side gates only. Low side is complementary 1 to high side gates with minimum internal dead
    time. -  What should I send to low side gates (controling like DRV8332?)

    Have a nice day

    Zbyno