Other Parts Discussed in Thread: TRS3221, MSP430F135, MAX3232
Hello, I'm trying to connect my MCU to RS232 ports.
This is the schematic.
I'm not using EK or DK board. The DOUT, RIN is connected to the RS232 pins using a USB to serial cable.
I'm trying to use the UART0 to echo my keyboard inputs to putty.
I used the UART-Echo example code from Tivaware.
However it doesn't work... No printing at putty. The example code is using PIOSC with 115200 baud rate.
Did I connected incorrectly?
The IC chip is TI TRS3221.