Hi
I use TMS470MF066HDK and IAR EWARM 7.10 with halcogen.
I have hard fault when starting debug.
Could you help me solve this problem.
No problem when the IDE was ccs5 or when IAR without Halcogen.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Somehow I could not open your project file. I created a new project and added the source files from your attachment. I did not get any Hard fault, Is there something I am missing while recreating your issue? Attached is the project I created. 2654.tmp.zip
Hi!
I uploaded the output file into the TMS470m using Uniflash and the program works fine.
But I still do not have the debug mode.
Hard Fault problem exactly associated with the emulator XDS100V2.
Perhaps IAR can not upload file into TMS470m using XDS100V2 or emulator does not operate normally with IAR and HALCOGEN.
Could you help me solve this problem.