This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SSI0 DMA Questions

Other Parts Discussed in Thread: TM4C123BH6ZRB

Hi,

I read a few discussions around the SSI DMA topic but didn't get the right information. I am using TM4C123BH6ZRB with IAR EWARM 6.50.5. I am using SSI0 Slave ISR and I was able to read and write fixed size 34 bytes messages to another micro-controller. The issue is reading 34-bytes from SPI Rx FIFO takes around 150us. I am trying to use DMA (from udma_demo and other posts) to minimize the time to read SPI Rx data register. My questions are:

1. TM4C123BH6ZRB data sheet states "Transfer size is programmable in binary steps from 1 to 1024". I can only set uDMAChannelTransferSet() with 32 or 64 but not 34 bytes?

2. I am testing out with a slow Rx data rate of incoming 32-bytes packet once every 2 seconds which follow by 32 0xFFs. It seems ping-pong configuration is way over kill but the Rx data is close (but not exactly) to my expectation. Should UDMA_MODE_BASIC or UDMA_MODE_AUTO work for this data rate?

3. With ping-pong configuration, I have the SPI ISR mode == UDMA_MODE_STOP. Half of the time, the data is close to what the sender sent out. The other half is zero.

4. On the better half of the messages, the received packets lost the first 2 bytes and appended with 2 zero bytes at the end.

Please see the attached files.

Thanks,

Dennis Nguyen

  • I also attach my data file.

  • Hello Dennis,

    1. No, the transfer size can be set for any value from 1-1024. The data sheets states binary steps and hence every value in this range is possible

    2. A Basic Mode would be OK for such data rates.

    3. I will go through the code and see if I can figure what is going on.

    Regards

    Amit

  • Hi Amit,

    I set the packet length to 34 bytes and I got DMA bus error. I changed to 32 bytes the DMA bus error went away. I am not sure what could be the problem.

    When I switched to basic mode, the SSI0 ISR is constantly interrupted with garbage data. In ping-pong mode, at least the data packets came in at the exact interval.

    In the mean time, I will turn my ADC ISR off to see if my SPI data getting any better,

    Thanks for your quick response to look at this.

    Dennis

  • Hello Dennis

    The error configuration which causes The DMA Bus Error is already a part of the zip code you have sent?

    Regards

    Amit

  • Yes. Thanks,

    Dennis

  • Hi Amit,

    I found the issue with DMA bus error. I think my ADC ISR took too long that causes SPI & DMA issues. By turning off ADC data processing I am no longer getting DMA bus error. Please consider item 1 is answered.

    Please advice on item 2-4.

    Thanks,

    Dennis

  • Hi,

    I actually found the DMA bus error is due my testing when I disable ADC initiailization but the TMR0 still active. I am trying to figure out item 3 and 4 and I found the behavior. I am using SSI2 master to communicate to a third micro-controller. This is a SSI blocking interface which write and read from SPI data registers. If I disable all write/read to SSI2, SSI0 Rx DMA is clean with the data rate of 250ms interval.

    When I crank up the SSI0 data to 200ms interval or faster, SSI0 Rx DMA buffer seems shifted after a while.

    Thanks for your inputs,

    Dennis Nguyen 

  • Hi,

    An alternate approach is for me to lower the SSI0 Interrupt than my ADC. Do you have any information to change the peripheral priority.

    Thanks,

    Dennis Nguyen

  • Hello Dennis,

    You can use IntPrioritySet to lower the priority but this will have affect only when the two interrupts come at the same time. If the CPU is processing a lower priority interrupt when a higher priority interrupt comes, then it will not drop the lower priority interrupt,

    Regards

    Amit

  • Thanks, Amit. I agree and I don't think lowering the priority will help me in this scenario. I am continuing to investigate the issue of SSI0 Rx DMA data buffer intefered by SSI2. I dumped the g_uDMAControlTable[1024]. All bytes are zeros except these offset: [180]-0x8,[181]-0x80,[182]-0,[183]-0x40,[184]-0xE5,[185]-0x43,[186]-0,[187]-0x20,[188]-0,[189]-0x80,[190]-0,[191]-0xC. Regradless, SSI2 traffic is on or not the content of g_uDMAControlTable is the same.

    My assumption was at the first step I am only interest for the SSI0 Rx packet. SSI0 Tx will be what ever in the Tx FIFO. With the issues existed I enable Tx uDMAChannelTransferSet in the ISR. My thought was missing Tx DMA might cause side effects. Just like my original provided code, I enable the following:

        if( !uDMAChannelIsEnabled( UDMA_CH11_SSI0TX ) )
        {
            //
            // Start another DMA transfer to TX.
            //
            uDMAChannelTransferSet( UDMA_CH11_SSI0TX | UDMA_PRI_SELECT,
                                        UDMA_MODE_BASIC, g_TxBuf,
                                        (void *)(SAF_SPI_BASE + SSI_O_DR),
                                        sizeof(g_TxBuf));

            //
            // The uDMA TX channel must be re-enabled.
            //
            uDMAChannelEnable( UDMA_CH11_SSI0TX );
        }

    With this Tx code enable, I got DMA error with g_uDMAControlTable all bytes are zeros except these offset: [180]-0x8,[181]-0x80,[182]-0,[183]-0x40,[184]-0xE5,[185]-0x43,[186]-0,[187]-0x20,[188]-13,[189]-0x82,[190]-0,[191]-0xC. Off set 188 and 189 are different. Please let me know the description of these 2 bytes.

    Thanks,

    Dennis

  • I checked with the data sheet and g_uDMAControlTable does not line up with my SSI0 configuration. I think I found the interfering with SSI2 problem. my g_uDMAControlTable was not aligned on 1024-byte boundary.