This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

errata_PBIST_4() function uses rsvd4[1] for TMS570LS0432 device

Other Parts Discussed in Thread: TMS570LS0432, HALCOGEN

Hello Support,
We are using TMS570LS0432 Corona Device which has only Port 0 for PBIST. There is no Port 1 for PBIST.

Hencec there is no FSRF1 Bit for Corona Device.
But in errata_PBIST_4() within Halcogen 3.08.01, I see that there is a check for pbistREG->rsvd4[1U] for the fault status check.
Can you please confirm if it is a mistake or not because I think that one is for PORT 1?

Thank you.
Regards
Pashan