Hi,
I am using a Tiva launchpad to display an image in GLCD. I burn my code using CCS. After debugging the code, I clicked the Run button. This made the code to execute and displayed something on the GLCD. But each time I had to connect the board to the PC, open CCS and click the run button to execute the program. Is there a way to run the program already present in the board to execute without the need of a PC ?