Other Parts Discussed in Thread: TMS570LS3137
Hi.
My question is regarding the TMS570LS3137.
In spnu499b.pdf, page 1718, chapter "32.2 Introduction", is stated:
"The eFuse controller automatically reads the values of the eFuses and shifts them into registers during the power-on reset sequence. ...
... the user code should check to see if a correctable or an uncorrectable error was detected during the reset sequence ..."
From this I understand that the ECC logic of the eFuse controller is active during the power-on reset sequence. That's clear.
I've now two questions:
* QUESTION 1: But is the ECC logic also permanently active AFTER the power-on reset sequence? I.e. does the ECC logic also checks the ECC checksum of those registers (to which the eFuse values were shifted to) permanently, even AFTER the power-on reset sequence finished?
* QUESTION 2: In case the ECC logic is permanently active: Would a correctable or an uncorrectable error, which happened AFTER the power-on reset sequence finished, also trigger the corresponding ESM channels (i.e. ESM group 1, channel 40, and/or ESM group 3, channel 1)?
I've also a third question:
* QUESTION 3: In case the ECC logic is NOT permanently active: Is there any mechanism with which could be detected that an unintended change of those registers (to which the eFuse values were shifted to) happened (e.g. cause of a bit flip)?
Reason for this 3rd question: IMHO a bit flip in one of those registers could lead to undesired system behaviour.
Thank you and regards
Oliver.