Other Parts Discussed in Thread: MAX3232, MAX232
Hello,
I have just initialized UART1 but it is not working there might be something missing out so I am posting my code so if any one can help me where is my initialization wrong?
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_can.h"
#include "inc/hw_adc.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/adc.h"
#include "driverlib/can.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
volatile int g_ui32Flags;
#ifdef DEBUG void __error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
void Timer0IntHandler(void)
{
char cOne, cTwo;
ROM_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
HWREGBITW(&g_ui32Flags, 0) ^= 1;
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, g_ui32Flags << 1);
ROM_IntMasterDisable();
cOne = HWREGBITW(&g_ui32Flags, 0) ? '1' : '0';
cTwo = HWREGBITW(&g_ui32Flags, 1) ? '1' : '0';
UARTprintf("\rT1: %c T2: %c", cOne, cTwo);
ROM_IntMasterEnable();
}
void Timer1IntHandler(void)
{
char cOne, cTwo;
ROM_TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
HWREGBITW(&g_ui32Flags, 1) ^= 1;
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, g_ui32Flags << 1);
ROM_IntMasterDisable();
cOne = HWREGBITW(&g_ui32Flags, 0) ? '1' : '0';
cTwo = HWREGBITW(&g_ui32Flags, 1) ? '1' : '0';
UARTprintf("\rT1: %c T2: %c", cOne, cTwo);
ROM_IntMasterEnable();
}
unsigned char a,b;
int main(void)
{
//Setting Clock
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
//Enabling UART1
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
GPIOPinConfigure(GPIO_PB0_U1RX);
GPIOPinConfigure(GPIO_PB1_U1TX);
GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//Configuring UART
UARTConfigSetExpClk(UART1_BASE,16000000, 9600, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
while(1)
{
UARTprintf("welcome\n");
// UARTCharPut(UART1_BASE,'d');
}
}