This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Discrepancy ot TRM spnu499b and Halcogen 03.08.00 code - CPU Reset Control Register

Other Parts Discussed in Thread: HALCOGEN

Hello,

the technical reference manual names a register at the address FFFF FFCCh as CPURSTCR. But within the Halcogencode this register is called as MMUGCR.

I guess that a description within TRM is a bit confusing:

"The CPURSTCR register shown in Figure 2-47 and described in Table 2-61, allows the memory protection

mode to be configured. It also allows a reset to the Cortex R4 CPU to be generated."

There are no user-accessible bits related to MPU.

Best regards,

Jiri