Other Parts Discussed in Thread: LM3S3748
Hi,
I am using the Tiva C series Launchpad to sample two channels and to display it in a GLCD for an oscilloscope project. I configured two ADC modules and initiated the sampling. The code is shown below. I will be needing only the MSB 6 bits of the ADC value. So I use a separate 8 bit word to store the values. But I am not able to display anything on the GLCD. When I try giving default values for the adcdata, I get a perfect sine wave. Please help me out.
void PortFunctionInit(void){
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); // Port A for control pins
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); // Port B for data pins
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD); // For ADC pins
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); // Port E for ADC inputs
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); // Port F for LED lights
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); // The ADC0 peripheral must be enabled for use.
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1); // The ADC1 peripheral must be enabled for use.
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_0); // Configuring PD0 as ADC input (channel 1) CH7 ADC0
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_1); // Configuring PD1 as ADC input (channel 2) CH6 ADC1
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_2); // Configuring PD2 as ADC input (time base) CH5
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_3); // Configuring PD3 as ADC input (trigger level) CH4
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0); // Configuring PE0 as ADC input (X-POS) CH3
}
int main(void)
{
uint8_t adc0data[128],adc1data[128];
uint32_t timebase,triglvl,xpos,adcbuffer[1],i;
SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); //20 MHz clock
PortFunctionInit();
GLCD_Initalize();
GLCD_ClearScreen();
uint8_t sinwav[128] = {0x20,0x25,0x2A,0x2F,0x33,0x37,0x3A,0x3C,0x3E,0x3F,0x3F,0x3E,0x3C,0x3A,0x36,0x32,0x2E,0x29,0x24,0x1F,0x19,0x14,0x10,0x0B,0x08,0x05,0x02,0x01,0x00,0x00,0x01,0x03,0x06,0x09,0x0D,0x12,0x17,0x1C,0x21,0x26,0x2B,0x30,0x34,0x38,0x3B,0x3D,0x3E,0x3F,0x3F,0x3D,0x3B,0x39,0x35,0x31,0x2C,0x28,0x22,0x1D,0x18,0x13,0x0E,0x0A,0x07,0x04,0x02,0x00,0x00,0x00,0x02,0x04,0x07,0x0A,0x0F,0x13,0x18,0x1D,0x23,0x28,0x2D,0x31,0x35,0x39,0x3C,0x3E,0x3F,0x3F,0x3E,0x3D,0x3B,0x38,0x34,0x30,0x2B,0x26,0x21,0x1C,0x16,0x12,0x0D,0x09,0x06,0x03,0x01,0x00,0x00,0x01,0x02,0x05,0x08,0x0C,0x10,0x15,0x1A,0x1F,0x24,0x29,0x2E,0x33,0x36,0x3A,0x3C,0x3E,0x3F,0x3F,0x3E,0x3C,0x3A,0x37};
/*while(1)
{
GLCD_ClearScreen();
for(i=64;i<128;i++)
GLCD_SetPixel(i,63-sinwav[i-64]);
for(i=0;i<63;i++)
GLCD_SetPixel(i,63-sinwav[i+64]);
for(i=0;i<1000;i++)
SysCtlDelay(1000);
}*/
ADCSequenceConfigure(ADC0_BASE, 2, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceConfigure(ADC1_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH5 | ADC_CTL_IE | ADC_CTL_END);
ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_CH5 | ADC_CTL_IE | ADC_CTL_END);
ADCSequenceStepConfigure(ADC1_BASE, 3, 0, ADC_CTL_CH4 | ADC_CTL_IE | ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, 2);
ADCSequenceEnable(ADC0_BASE, 3);
ADCSequenceEnable(ADC1_BASE, 3);
ADCIntClear(ADC0_BASE, 2);
ADCIntClear(ADC0_BASE, 3);
ADCIntClear(ADC1_BASE, 3);
while(1)
{
ADCIntClear(ADC0_BASE, 2);
ADCProcessorTrigger(ADC0_BASE, 2); // Trigger the ADC conversion.
while(!ADCIntStatus(ADC0_BASE, 2, false)){} // Wait for conversion to be completed.
ADCIntClear(ADC0_BASE, 2); // Clear the ADC interrupt flag.
ADCSequenceDataGet(ADC0_BASE, 3, adcbuffer); // Read ADC Value.
timebase = adcbuffer[0];
for (i=0;i<128;i++)
{
ADCIntClear(ADC0_BASE, 3);
ADCIntClear(ADC1_BASE, 3);
ADCProcessorTrigger(ADC1_BASE, (3|ADC_TRIGGER_WAIT)); // Put ADC-1 in Trigger Wait
ADCProcessorTrigger(ADC0_BASE, (3|ADC_TRIGGER_SIGNAL)); // Put ADC-0 in Global Trigger
while(!ADCIntStatus(ADC0_BASE, 3, false)){} // Wait for conversion to be completed.
ADCIntClear(ADC0_BASE, 3); // Clear the ADC interrupt flag.
ADCIntClear(ADC1_BASE, 3); // Clear the ADC interrupt flag.
ADCSequenceDataGet(ADC0_BASE, 3, adcbuffer); // Read ADC Value.
adc0data[i] = adcbuffer[0]>>8;
ADCSequenceDataGet(ADC1_BASE, 3, adcbuffer); // Read ADC Value.
adc1data[i] = adcbuffer[0]>>8;
}
GLCD_ClearScreen();
for(i=0;i<128;i++)
{
GLCD_SetPixel(i,adc0data[i]);
GLCD_SetPixel(i,adc1data[i]);
}
}
}
Regarding the code, the array sinwav is just a sample waveform which will be used by the commented code right next to it to check if a sine wave can be displayed on the GLCD.
Thanks in advance.