This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570 ADC Input Range

Hello,

As you know, TMS570 has ADREFHI and ADREFLO inputs  to map analog inputs into 0x0 - 0xFFF. In most applications, ADREFHI is connected to +5V or +3V and ADREFLO to GND. Instead of these, is it possible to directly read bipolar inputs (-5V to +5V   or -3V to 3V) by connecting ADREFLO to -5V or - 3V. If yes, this will eliminate the shifting opamp circuits.

Thank you,