This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timer count edges and sync a output match without interrupt



Hello Forum,


I allready set up the Timer to count falling and raising edges at 17 MHz (there is room for two cpu cycles at 120 MHz). Now it would be fine to set a compare match output sync'ed to the 17 MHz signal... (Interrupt would be to slow!)

Is there any solution? (I allready checked the Datasheet... )


Thx for help


-Basti

  • Hello Sebastian

    So when the number of edges are counted equal to the programmed value, you would want to have a GPIO toggled by the timer w/o CPU going to the interrupt handler and then toggling an output GPIO?

    If that is the case, then it is not possible directly. You may use DMA but it would also involve delay.

    Regards

    Amit

  • Hello Amit,

    thx for your fast response.

    Okay, I tought as much.

    I have to use fast AC logic gates for my solution... I notice that sampling at TI issn't possible for this stuff :(

    But thats another story...

    Thanks for your great help!

    -Basti