This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem of TM4C129x spi clock

Asked for help from what I got yesterday.

so i try to spi communication, but it is still not work.

upside picture is idle situation. downside picture is my situation.

i can check every line is well. but clk is have problem. how can i make keep clk until the end of the receive action

int

main(void)

{

    tContext sContext;

    uint32_t ui32SysClock;

    ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |

                                       SYSCTL_OSC_MAIN |

                                       SYSCTL_USE_PLL |

                                       SYSCTL_CFG_VCO_480), 120000000);

    PinoutSet();

    Kentec320x240x16_SSD2119Init(ui32SysClock);

    GrContextInit(&sContext, &g_sKentec320x240x16_SSD2119);

    FrameDraw(&sContext, "Radar Test");

    GrContextFontSet(&sContext, g_psFontCm48);

    GrStringDrawCentered(&sContext, "using spi", -1,

                         GrContextDpyWidthGet(&sContext) / 2,

                         ((GrContextDpyHeightGet(&sContext) - 32) / 2) + 24,

                         0);

    GrFlush(&sContext);

uint32_t pui32DataTx[NUM_SSI_DATA];

       uint32_t pui32DataRx[NUM_SSI_DATA];

       uint32_t ui32Index;

 //      InitConsole();

          SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);

          SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);

          GPIOPinConfigure(GPIO_PD3_SSI2CLK);

          GPIOPinConfigure(GPIO_PD2_SSI2FSS);

          GPIOPinConfigure(GPIO_PD1_SSI2XDAT0);

          GPIOPinConfigure(GPIO_PD0_SSI2XDAT1);

          GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 |

                         GPIO_PIN_3);

          SSIConfigSetExpClk(SSI2_BASE, ui32SysClock/14, SSI_FRF_MOTO_MODE_0,

                             SSI_MODE_MASTER, 1000000, 16);

          SSIEnable(SSI2_BASE);

          while(SSIDataGetNonBlocking(SSI2_BASE, &pui32DataRx[0]))

          {

          }

          pui32DataTx[0] = 0x0103;

          pui32DataTx[1] = 0x0101;

          //pui32DataTx[2] = 0x0000;

          //pui32DataTx[3] = 0x0000;

          for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)

          {

              SSIDataPut(SSI2_BASE, pui32DataTx[ui32Index]);

          }

          while(SSIBusy(SSI2_BASE))

          {

          }

          for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)

                              {

                                 SSIDataGet(SSI2_BASE, &pui32DataRx[ui32Index]);

                              }

  while(1){

}

}