Greetings,
I'm currently trying to interface my Tiva C Series with a Sparkfun Breakout Board, IMU Digital Combo Board - 6 Degrees of Freedom ITG3200/ADXL345 and I'm having trouble with the I2C interface.
currently this is my code:
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/i2c.h"
uint8_t SLAVE_ADDRESS = 0x68;
uint32_t first_byte, second_byte, temperature, result;
void i2c_setup(void) {
//Enable the I2C Module
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C2);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
//Wait at least 5 clock cycles
SysCtlDelay(2);
//Configure SDA and SCL
GPIOPinConfigure(GPIO_PE4_I2C2SCL);
GPIOPinConfigure(GPIO_PE5_I2C2SDA);
//Wait at least 5 clock cycles
SysCtlDelay(2);
//Set PE4 as SCL
GPIOPinTypeI2CSCL(GPIO_PORTE_BASE, GPIO_PIN_4);
//Set PE5 as SDA
GPIOPinTypeI2C(GPIO_PORTE_BASE, GPIO_PIN_5);
//Configure Master,
I2CMasterInitExpClk(I2C2_BASE, SysCtlClockGet(), false);
}
uint32_t i2c_read() {
I2CMasterSlaveAddrSet(I2C2_BASE, SLAVE_ADDRESS, false);
I2CMasterDataPut(I2C2_BASE, 0x1A);
I2CMasterControl(I2C2_BASE, I2C_MASTER_CMD_SINGLE_SEND);
while(I2CMasterBusBusy(I2C2_BASE)); //Loop until the bus is no longer busy
I2CMasterSlaveAddrSet(I2C2_BASE, SLAVE_ADDRESS, true );
I2CMasterControl(I2C2_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
while(I2CMasterBusBusy(I2C2_BASE)); //Loop until the bus is no longer busy
first_byte = I2CMasterDataGet(I2C2_BASE);
return first_byte;
}
void setup()
{
Serial.begin(9600);
i2c_setup();
}
void loop()
{
int test = i2c_read();
Serial.println(test);
delay(1000);
}
I'm using Energia to test my program, and when I try to read from the specified register, I get the same result, no matter which register I choose, the result is always decimal 229 (this is the Accelerometer's Device Address).
Can somebody point me in the right direction, I've been looking at my code for quite some time and still don't know whats wrong...
Thanks!