Other Parts Discussed in Thread: TM4C123GH6PM
Hi there,
so I am trying to run my tiva c in usb host mode in order to connect a usb stick to the board, however i run into my faultISR on this line :
GPIOPinTypeUSBDigital(GPIO_PORTH_BASE, GPIO_PIN_3 | GPIO_PIN_4);
when i try to run the code from the tivaware usb manual
//
// Enable Clocking to the USB controller.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_USB0);
//
// Enable the peripherals used by this example.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH);
//
// Set the USB0EPEN and USB0PFLT pins to be controlled by the USB
// controller.
//
GPIOPinTypeUSBDigital(GPIO_PORTH_BASE, GPIO_PIN_3 | GPIO_PIN_4);
//
// Register the host class drivers.
//
USBHCDRegisterDrivers(0, g_ppsUSBHostClassDrivers,
g_ui32NumHostClassDrivers);
//
// Call any open routines on the device class interfaces here so that they
// are ready to receive callbacks if the device is already inserted on
// power on.
//
USBHMSCDriveOpen(0, MSCCallback);
//
// Initialize the host controller.
//
USBHCDInit(0, g_pui8HCDPool, HCD_MEMORY_SIZE);
tUSBHMSCInstance* device = USBHMSCDriveOpen(0, mscCallback);
while(USBHMSCDriveReady(device)) {
}
printf("Done initializing.\n");
I read something about 0-ohm resistors that need to be present for otg/host mode to work, is this related to my problem? If so, how would I go about attaching them to R25 and R29 on my tiva c?
Sorry If this sounds very newbish, however it is one of my first mc projects.
Thanks for the help.