Hello Amit!
In my last post, you send to me working UART uDMA code, which receive Data from PC.
Can you a little bit more explain, how you tested/send data to Launchpad?
Today I'm all day trying it, sending longer than 16 characters data via Putty program or Terminal v1.9b, buffers still empty..
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "driverlib/udma.h"
#include "utils/cpu_usage.h"
#include "utils/uartstdio.h"
#include "utils/ustdlib.h"
//*****************************************************************************
//*****************************************************************************
#if defined(ewarm)
#pragma data_alignment=1024
uint8_t ui8ControlTable[1024];
#elif defined(ccs)
#pragma DATA_ALIGN(ui8ControlTable, 1024)
uint8_t ui8ControlTable[1024];
#else
uint8_t ui8ControlTable[1024] __attribute__ ((aligned(1024)));
#endif
#define UART_TXBUF_SIZE 16
#define UART_RXBUF_SIZE 16
static uint8_t g_pui8TxBuf[UART_TXBUF_SIZE];
static uint8_t g_pui8RxPing[UART_RXBUF_SIZE];
static uint8_t g_pui8RxPong[UART_RXBUF_SIZE];
// Error counter
static uint32_t g_ui32DMAErrCount = 0;
// Transfer counters
static uint32_t g_ui32RxPingCount = 0;
static uint32_t g_ui32RxPongCount = 0;
volatile int UARTIntHitsCounter = 0;
// uDMA control table aligned to 1024-byte boundary
#pragma DATA_ALIGN(ucControlTable, 64)
uint8_t ucControlTable[64];
void
uDMAErrorHandler(void)
{
uint32_t ui32Status;
ui32Status = ROM_uDMAErrorStatusGet();
if(ui32Status)
{
ROM_uDMAErrorStatusClear();
g_ui32DMAErrCount++;
}
}
// UART interrupt handler. Called on completion of uDMA transfer
void
UART0IntHandler(void)
{
uint32_t ui32Status;
uint32_t ui32Mode;
ui32Status = ROM_UARTIntStatus(UART0_BASE, 1);
ROM_UARTIntClear(UART0_BASE, ui32Status);
UARTIntHitsCounter++;
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT);
if(ui32Mode == UDMA_MODE_STOP)
{
g_ui32RxPingCount++;
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART0_BASE + UART_O_DR),
g_pui8RxPing, sizeof(g_pui8RxPing));
}
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT);
if(ui32Mode == UDMA_MODE_STOP)
{
g_ui32RxPongCount++;
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART0_BASE + UART_O_DR),
g_pui8RxPong, sizeof(g_pui8RxPong));
}
if(!ROM_uDMAChannelIsEnabled(UDMA_CHANNEL_UART0TX))
{
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_pui8TxBuf,
(void *)(UART0_BASE + UART_O_DR),
sizeof(g_pui8TxBuf));
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART0TX);
}
}
// Initialize UART uDMA transfer
void
InitUART1Enable(void)
{
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
// Enable UART1 and make sure it can run while the CPU sleeps
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART0);
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
// Configure and enable the UART with DMA
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 115200,
UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE);
ROM_UARTFIFOLevelSet(UART0_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);
ROM_UARTEnable(UART0_BASE);
ROM_UARTDMAEnable(UART0_BASE, UART_DMA_RX);
ROM_IntEnable(INT_UART0);
// Receive channel setup for ping and pong
ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART0RX,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_UART0RX,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART0_BASE + UART_O_DR),
g_pui8RxPing, sizeof(g_pui8RxPing));
ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART0RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART0_BASE + UART_O_DR),
g_pui8RxPong, sizeof(g_pui8RxPong));
// Enable both channels
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART0RX);
}
int
main(void)
{
volatile uint32_t ui32Loop;
ROM_FPULazyStackingEnable();
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
ROM_SysCtlPeripheralClockGating(true);
// GPIO setup for LEDs
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2);
// Enable uDMA
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_UDMA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
//ROM_IntEnable(INT_UDMAERR);
ROM_uDMAEnable();
ROM_uDMAControlBaseSet(ucControlTable);
// Initialize the uDMA/UART
InitUART1Enable();
while(1)
{
if(UARTIntHitsCounter > 0)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2);
SysCtlDelay(SysCtlClockGet() / 20 / 3);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0);
SysCtlDelay(SysCtlClockGet() / 20 / 3);
}
}
}
at startup_ccs
extern void uDMAErrorHandler(void);
extern void UART0IntHandler(void);
IntDefaultHandler, // GPIO Port E
UART0IntHandler, // UART0 Rx and Tx
uDMAErrorHandler, // uDMA Error
IntDefaultHandler, // uDMA Software Transfer uDMAIntHandler