This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HET_IDE: avoid conflict with two programs



Hi,

I'm developing an application for RM48 that uses two different custom codes for the two HETs.

Both HET programs are assembled with HET_IDE and the generated .c and .h are included in the CCS code.

The problem is that both assembled codes uses the same define (HETPROGRAM0_UN, HET_INIT0_PST, ecc) causing a clear conflict in the code compilation.

There is a way to modify the HET_IDE behaviour and to change the define labels?

thank you,

Matteo

  • Thanks for using the Hercules forum! An engineer has been notified of your question.

  • Matteo,

    Yes and no....

    The het assembler 'hetp' takes -hc32 -nX as an option where X is a # 0,1,2,...

    If you use -hc32 -n1 on the command line, instead of HETPROGRAM0_UN you'll get HETPROGRAM1_UN in the output.

    So that's how you assembly differently for the two different N2HETs.

    But I just tried simply adding the -hc32 -nX on the 'options' of the HET IDE where the executable path is.  It doesn't work and in fact crashes so I wouldn't try it.

    I think you may be at a point where you can consider building your programs separately - let the HET IDE build them for testing in the HET IDE, but then assemble them again in with the correct options either through CCS or through a makefile.

    CCS does let you add custom build steps so you could use this mechanism to assemble each of your HET programs before the rest of your applicaton builds.

  • Very clear, thank you.