Hi,all
I have two questions for the ADC.
(1) Assume Event Group Request has occurred during sampling of Group1.
(A) Sampling of Group1 is suspended, sampling of the Event Group will begin then?
(B) After sampling of Group1 has finished, sampling of Event Group begins?
Which is correct of (A) or (B)?
I think (B) is correct.
(2) Assume (B) is correct.
I have an understanding of the following
Please tell me if there is a mistake.
Suppose that channels 0, 1, and 2 are selected for conversion in the Event Group, channels 4, 7, and 8
are selected for conversion in group 1, and channels 3, 5, and 6 are selected for conversion in group 2.