This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Port on T4MC1294 Connected LaunchPad



Hi, I want to use Ethernet with 80 GPIOS input/output on Connected LaunchPad, so is is possible ?
and Connected LaunchPad can uses in industrial environments?
Thanks !

  • Cuong Mai Manh Khanh said:
    Hi, I want to use Ethernet with 80 GPIOS input/output on Connected LaunchPad, so is is possible ?

     Connected launchpad is a development board, if you can access all pin you need answer is yes.

    Cuong Mai Manh Khanh said:
    and Connected LaunchPad can uses in industrial environments?

     This board as long as you can do ceritication with FCC or CE, to other recomandation are mandatory to the final use can be yes.

     A development board never is industrial nor commercial/domestic/professional use certified for an unknown application.

     Development board serve as development aid of some prototype.