Other Parts Discussed in Thread: TM4C1233H6PZ
I'm working with a TM4C1233H6PZ on a custom board. My debugging environment consists of CCS 5.4 and a XDS200 interface.
I'm investigating on following issue: I have a sample code, overall the usb_dev_serial of tivaware_C_Series 1.1, which emulates a CDC device. If I'm running my code on a "blank" device within the debugging environment the PC side enumerates and I'm getting a new virtual COM port at the PC side. Also a terminal emulation is working without any problems. After a power cycle I run the code equally in my debugging environment, but the PC enumerates not any more. The cpu is till running. I can observe this by a software controlled blinking LED. Only a flash erase in CCS gets the device back to enumerate on the next run until the next power cycle ...
Another miracle behaviour to me, which is obviously in correlation with the first issue, is the fact that the blank device only enumerates as a DFU device, if the XDS200 debugger is plugged, also the CCS is not running. If I cut the XDS 200 connection the Stellaris Device Firmware Update disappears out of the device manager.
Are there any hints to troubleshooting this issue? Which influence has the XDS200 on the device?
Best regards
Thomas Rapolder