This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN dominant bit



Hi everybody.

I don't have any experience with CAN interface.

I used examples and documentation. So my Tiva C launchpad succesfully transmit and recive messages now.

But I have one question for which I didn't find an answer in docs. Which bit in CAN module is dominant: hardware "0" or "1" in message's ID?

I mean which ID will win arbitration in CAN bus: 0x000 or 0xFFF?