Error connecting to the target:
(Error -154 @ 0x0)
One of the FTDI driver functions used to
write data returned bad status or an error.
(Emulation package 5.0.747.0)
so I tried resetting and unplugged-plugged the connections, but still got the same error message, the error message was not there two days ago, and the project run successfully. But now with the exact same project, I got this error, could someone possibly know the solution?
Thanks