Other Parts Discussed in Thread: RM46L430
Hi,
With regards to RM46L430 errata, there are few Cortex-R4 related problems
and we need some advice about "CORTEX-R4#46".
This errata mentions that "The operation to prefetch an instruction by MVA,
as defined in the ARMv6 architecture" a CP15 accesses may generate an UNDEFINED exception.
The instruction is "MCR p15,0,<Rt>,c7,c13,1 ; NOP".
We would like to know, in case of a practical application where exactly this
errata could effect?. We don't know how to find out if our application program is affected by this errata,
Do we have to explicitly write a assembly code(above) in order to see this error?
I tried to ask the same question on the ARM forum
but there was no reply only...
http://community.arm.com/message/18792#18792
So I am posting here hoping some advice from the TI support.
Best Regards.
Prad