Other Parts Discussed in Thread: BOOST-CCEMADAPTER
Hello,
I have a simple question:
Sharp LCD BoosterPack (430BOOST-SHARP96) for the LaunchPad is compatible with Tiva TM4C123G Launchpad?
Thanks.
Regards,
Antonino Proto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BOOST-CCEMADAPTER
Hello,
I have a simple question:
Sharp LCD BoosterPack (430BOOST-SHARP96) for the LaunchPad is compatible with Tiva TM4C123G Launchpad?
Thanks.
Regards,
Antonino Proto
Hello Antonino
The Pin out for the Booster Pack does not match that on Tiva LaunchPad for the following
1. The AIN chnanels needed for the slider is not compatible
2. The SSI_FSS is not mapped to the SPI_CS. Instead you may have to use the GPIO as SSI_CS by manually making it low before a SSI Transmit and then drive it high.
Regards
Amit
Hello Amit,
thanks for quick repsonse.
Therefore, step 2 is correctable using the GPIO as SSI_CS by manually making it low before a SSI Transmit and then drive it high.
Step 1 is it fixable with BOOST-CCEMADAPTER - EM Adapter BoosterPack? (https://estore.ti.com/boost-ccemadapter.aspx)
Thanks.
Regards,
Antonino
Hello Antonino,
Please go through the following page. It will list out booster packs based on the MCU.
http://www.ti.com/ww/en/launchpad/boosterpacks.html
I am not too familiar with the EM Adapter Booster Pack and will need to study the schematics as well.
Regards
Amit