i insert 1 bit error in ram, and it will indicate corresponding error in ram wrapper register. but error was not indicate ESM. i don’t know why? thank u!!!
(but ESM register do not have error been indicated)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ron,
Looking through our internal docs, I believe the ESM signal is the same as the interrupt, and I see that the interrupt isn't enabled. You might try enabling the interrupt in the ram wrapper to see if that makes the error also propogate to the ESM. (Since this is a single bit correctable error).
You never answered Anthony's question about the part number of the micro you are using. It make a difference where the ECC is being checked, and I am pretty sure it varies by part.
If the ECC is being checked by the CPU and the event bus export is not enabled it cannot send a signal to the ESM when there is an error.
From app note SPNA106D:
Enable the Cortex-R4F CPU’s Event Signaling Mechanism
The Cortex-R4F CPU has a dedicated event bus that is used to indicate that an event had occurred. This
event signaling is disabled upon reset and must be enabled. The Flash module and the RAM module
interfaces capture the ECC error events signaled by the CPU. This allows the application to further debug
the exact address, which caused the ECC error.
The CPU event signaling can be enabled by setting the “X” bit of the performance monitoring unit’s
“Performance monitor control register, c9”.