Dear all,
I have been observing the same behaviour as described in this forum thread. But a disconnection of the JTAG ribbon has not helped because my scenario and conditions are a bit different. Actually a following point 1) is successfully finished even if the JTAG is plugged in.
1) perform ccmSelfCheck() - successfully done,
2) force to a global system reset by writting into SYSECR register,
3) ccmSelfCheck() is called again but waits for finishing the selftest forever.
I suspect the point 2) is the reason of this behaviour, am I right? Between the points 2) and 3) there is further code executed - should I check another setting which could causes such issue?
Note: If the point 1) is omitted the behaviour does not change - still stuck.
Many thanks in advance,
best regards, Jiri