Other Parts Discussed in Thread: HALCOGEN, RM46L852
iHi,
I'm working on a robotic project that uses two or possibly more motor controller MCUs which need to be connected through a serial interface. The system must also be connected through Ethernet. Some peripherals are connected through a 400khz I2C bus. My request is the list of pins to enable in Halcogen or better yet a Halcogen file :)
I saw that SCI and SCILIN pins are present but the debugger uses SCILIN. Are there any more serial interfaces available? If not what are the other options to debug?